JOKARI is a highly highly specialised manufacturer of insulation strippers. The brand's history dates back to 1949, when the company began its business as a small electrical shop. JOKARI remains a family-owned company and takes pride in the fact that its products are still manufactured locally, exclusively in Germany, using high-quality materials.
Among the wide range of wire stripping products (available directly from TME warehouses), you will find a set that should satisfy the needs of any electrical installer, fitter or maintenance technician. The JO90810 set is a selection of JOKARI tools enclosed in a lightweight, convenient hardcase with a handle. The set includes products listed below.

functional stripping tool.
JOKARI 10282
The body of the JOKARI cable knife is made of extremely wear-resistant polyamide. It is designed for stripping insulation from all standard round cables. The sheath cutting depth is set using a knob placed at the end of the handle. The knife is a perfect tool for stripping the outer insulation of multicore cables, e.g. when making connections in a fuse box. With this tool, you can perform two basic operations: making an omnidirectional cut and a longitudinal cut.

a fine adjustment of the stripping
depth and a chisel blade.
JOKARI 20050
An ergonomic automatic insulation stripper designed for cables with a cross-sectional area ranging from 0.2mm2 to 6.0mm2. It is a perfect tool for removing insulation in a fast and precise way, even in hard-to-reach places. The tool is equipped with a stripping distance limiter and a built-in chisel blade with a long lever. The design of the tool allows stripping of both solid-core and stranded-core wire – which minimises the likelihood of conductor damage (and therefore: of a dangerous increase in cable resistance).
JOKARI 30900

insulation stripper by JOKARI.
T30900 is a simple, multi-purpose tool for stripping insulation from all standard round cables, which makes it an ideal choice for work with systems installed in buildings, industrial parks , as well as those applied in telecommunication or solar systems. The tool has a number of holes and several blades, as well as a limiter – thanks to this, it can also be used for work with flat and coaxial cables.
Parameters | |
---|---|
Tool type: | set |
Tool application: | cable insulation stripping |
Cable type: | round, flat |
Target group: | fitters |
Packaging type: | hardcase |